Pulse Building

Antenna Pattern Types

Antenna Pattern Type sets the pattern type for the antenna scan. Each type has specific properties that control its behavior. Changing the antenna pattern type causes the scan properties to be reset to their default values.

Available antenna scan pattern types are:

Antenna Pattern Type Description Visual Configuration
None No antenna scan modulation is applied to the pulse pattern.  
Circular

The antenna beam rotates in a circular motion.

The following property is used with this Type:

Scan Rate

 

Conical

The antenna beam rotates in a cone-shaped pattern.

The following properties are used with this Type:

  • Scan Rate

  • Cone Radius

 

Custom

A custom amplitude pattern is provided by importing a file containing amplitude data. The file format is ASCII CSV and the data is assumed to be in dB. The valid data range is from -100 dB to 0 dB. Time is assumed to be constant and equal between data points. It is assumed that the file contains one complete scan of the amplitude pattern. The time increment between data points is established using the scan rate property. The Custom amplitude pattern is not combined with any other antenna properties except Null Depth. The maximum dynamic range of the amplitude pattern is hardware specific and most likely less than 100 dB.

The following properties are used with this Type:

  • Scan Rate

  • Interpolation

  • User File Name

The following properties are not available for this Type:

  • Radiation Type

  • Receiver Location

  • Horizontal Beam Width

  • Vertical Beam Width

Bidirectional Raster

The antenna beam sweeps back and forth across a raster grid.

The following properties are used with this Type:

  • Scan Rate

  • Retrace Time

  • Raster Width Angle

  • Bar Width Angle

  • Number of Raster Bars

  • Beam On Retrace

 

Unidirectional Raster

The antenna beam sweeps in one direction across a raster grid, then returns to the start.

The following properties are used with this Type:

  • Scan Rate

  • Retrace Time

  • Raster Width Angle

  • Bar Width Angle

  • Number of Raster Bars

  • Fly Back Time

 

Bidirectional Sector

The antenna beam sweeps back and forth within a defined sector angle.

The following properties are used with this Type:

  • Scan Rate

  • Sector Width Angle

 

Unidirectional Sector

The antenna beam sweeps in one direction within a sector, then returns without scanning.

The following properties are used with this Type:

  • Scan Rate

  • Sector Width Angle

  • Flyback Time